AIN#.VALUE

Description

AIN#.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).

Examples

Code

--> AIN1.VALUE
1.420 V

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units V
Range -12.5V to +12.5V
Default Value N/A
Data Type Float
See Also  
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AIN1.VALUE

3780h

01h

Signed16

-

1000:1

Read only

Yes

AIN2.VALUE

3781h

01h

Signed16

-

1000:1

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

23100

1

23100 (0x5a3c)

AIN1.VALUE

Signed16

Read Only

Yes

23101

1

23101 (0x5a3d)

AIN2.VALUE

Signed16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AIN1.VALUE

23100

Float

Read Only

-

AIN2.VALUE

23101

Float

Read Only

-